Cancel
Showing results for 
Search instead for 
Did you mean: 

FSC Server failed to start

Genius
Genius

Hello all

 

I update TC 11.2.3 to 11.3

It shows me wrong message

My FSC service can't start

2.PNG

 

How can I solve this problem?

Where I need to change file?

 

 

Best Regards

 

 

Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10
4 REPLIES

Re: FSC Server failed to start

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

copied this from GTAC:

looks like the user is infodb and not infodba.

xtof

 

To correct the user, modify the configuration.xml file so that the correct 
user name is granted access to the FSC Service.  Make sure the installing user 
and the OS user.

EXAMPLE:
<installingUser value="user1" />

AND

<OSUser>
   <password value="PASSWORD" />
   <user value="infodb.srv" />
</OSUser>

 

Re: FSC Server failed to start

Genius
Genius

Hello,

 

I found Configuration.xml and copy error line

I used infodba account to install TC

When this error show up FSC service will dispear

 

I upload tcf.zip file include

1.install_UPDATER.log

2.Configuration.xml

 

rocessing 'patch' for config1/FMS Server Cache
Time: Fri Aug 25 11:59:32 CST 2017
===============================================
Deleting directory C:\Teamcenter11/fsc/third_party/commons-collections/3.0, recurse: true
Running com.teamcenter.install.tceng.fms.fsc.Fsc
Checking for FSC installation in configuration 'config1'
Starting service FSC service
Installing FMS service (Windows)
Service Teamcenter FSC Service FSC_tct_infodba will be stopped/removed
Stopping service
Removing service

Executing [cd /D "C:\Teamcenter11"]
Output from command: cd /D "C:\Teamcenter11"
command_exit=0
Exit Status 0, elapsed time 0:00:00
Converting C:\PROGRA~1\Java\jre7 to UNC path
Converting C:\Teamcenter11\fsc to UNC path

Executing ["C:\Teamcenter11\fsc\installfsc.bat" "C:\PROGRA~1\Java\jre7" "C:\Teamcenter11\fsc" FSC_tct_infodba]
Output from command: "C:\Teamcenter11\fsc\installfsc.bat" "C:\PROGRA~1\Java\jre7" "C:\Teamcenter11\fsc" FSC_tct_infodba
--------
Usage: "C:\Teamcenter11\fsc\installfsc.bat" jdk_home FSC_HOME FSCID
Example: "C:\Teamcenter11\fsc\installfsc.bat" %JAVA_HOME% %FSC_HOME% myfsc
Note, if JAVA_HOME or FSC_HOME contain spaces, they must be quoted on the command line.
--------
The Teamcenter FSC Service FSC_tct_infodba automatic service was successfully installed.
command_exit=0
Exit Status 0, elapsed time 0:00:00
Granting user 'TCT\infodba' SeServiceLogonRight right
An error occurred during execution. Stack trace follows...
com.teamcenter.install.tceng.fms.fsc.Fsc.windowsInstall(Fsc.java:518)
com.teamcenter.install.tceng.fms.fsc.Fsc.patchFSC(Fsc.java:645)
sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
java.lang.reflect.Method.invoke(Unknown Source)
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:209)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:135)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:201)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:181)
com.teamcenter.install.tem.patch.Patch.processPatchTasks(Patch.java:1094)
com.teamcenter.install.tem.patch.Patch.processPatchTasks(Patch.java:781)
com.teamcenter.install.tem.patch.Patch.finish(Patch.java:446)
com.teamcenter.install.tem.patch.Patch.begin(Patch.java:294)
com.teamcenter.install.tem.director.actions.PatchingAction.execute(PatchingAction.java:47)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:143)
com.teamcenter.install.tem.director.Director.run(Director.java:134)
java.lang.Thread.run(Unknown Source)
***
*** CANCELLED
***
=====================================================
Installation interrupted due the following reason:

UPDATE MANAGER FAILURE: PatchingAction: Patch task failed while processing feature, 'FMS Server Cache': Service 'Teamcenter FSC Service FSC_tct_infodba' failed to start due to:LookupAccountName: 1332
Time: Fri Aug 25 13:10:26 CST 2017
=====================================================

=====================================================
CommentStore
=====================================================
Configuration update failed: config1: Patch task failed while processing feature, 'FMS Server Cache': Service 'Teamcenter FSC Service FSC_tct_infodba' failed to start due to:LookupAccountName: 1332
Severity: 1 (Severe)

An internal error occured which has caused processing to stop.
Severity: 1 (Severe)

Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10

Re: FSC Server failed to start

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

TEM is failing while trying to grant user TCT\infodba "Log on as a service" rights. It fails trying to find (lookup) the user TCT\infodba. Does the user "infodba" exist in domain "TCT"?

 

You might be able to find out why the lookup fails by doing it manually.
Computer Configuration\Windows Settings\Security Settings\Local Policies\User Rights Assignment

Double-click "Log on as a service"

 

See attached doc for screen shots. Once you're able to assign TCT\infodba the "Log on as a service" right then you can go back to TEM and try again.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: FSC Server failed to start

Genius
Genius
Hello RandyEllsworth,

Thank you for help.
I found the problem is!
I use active directory,so I need to change service account.
I change Configuration.xml file TCT\\infodba to CADEX\\infodba.
And change all TC service account from .infodba to CADEX\infodba retry again.
It Works!
Problem Solve!
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10