Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Failed to Validate the Version for License

Genius
Genius
Hello ardenb

YES,I can ping YY when I installing TC.
But It seen firewall stop connect TC to YY
Now I am looking for where the problem is.
Thank you.
Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10

Re: Failed to Validate the Version for License

Gears Phenom Gears Phenom
Gears Phenom

I had a license error last week but my error message was different. It was the firewall blocking the ports. I had to declare the port and add the port into the license file to make it work for me.

 

My error:

lic.jpg

 

Add to license flie:

SERVER SERVERHOSTNAME COMPOSITE=COMPHOSTID 28000                                        

VENDOR ugslmd PORT=26999

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC
Highlighted

Re: Failed to Validate the Version for License

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The bottom line is that you have a communication problem. TEM isn't able to get a response from the license server. And there are zero entries in the splm log that indicate anyone is talking to it. Most likely this is a firewall issue which can be tested by temporarily turning off the firewall and running TEM again. If disabling the firewall worked then you can proceed as below...

The license server is listening on port 28000 so naturally you would add 28000 to the firewall exceptions. The "answer" port, if not specified, is a range of ports which makes creating a firewall exception difficult. You can force answering to be on a specific port by adding an argument to the VENDOR line in the license file...

SERVER YY COMPOSITE=nnnnnnnnn 28000
VENDOR ugslmd PORT=28005

Restart the license service on YY after modifying the license file. Open ports 28000 (listen) and 28005 (answer) in the YY firewall.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Failed to Validate the Version for License

Genius
Genius

Hello All

 

Thank you for all comments.

The problem is:

1.Firewall

It stop port to get and answer

2.License

I renew license

 

Now the problem solve.

 

Thank you all.

Best Regard.

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10

Re: Failed to Validate the Version for License

Creator
Creator

Where is license file for Teamcenter?

I am installing TC and currently getting the error "Failed to validate the version for license server 28000@PC430355. Return value = -15"

Re: Failed to Validate the Version for License

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
The license is likely in the same folder as lmgrd.exe/ugslmd.exe called splm9.lic (or similar). Note: your license log will also be in that folder called splm_ugslmd.log. Check the properties of the service running on PC430355 to find where the exe's are located.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Failed to Validate the Version for License

Creator
Creator

I just installed TC 4 tier and standalone BMIDE in my local machine and while logging for the first time I am getting an error:

 

com.teamcenter.soa.client.SoaRuntimeException: Failed to send the service request, encountered an HTTP I/O error.

sun.security.validator.ValidatorException: PKIX path building failed.

sun.security.provider.certpath.SunCertPathBuilderException: Unable to find valid certification path to requested target.

 

I could not locate my TCDATA, I am doing something wrong?

If I am selecting the option TC 2tier+BMIDE stanalone+Corporate server I am getting licence file error.

What options should I select for hassle free TC 2 tier install???

 

 

Re: Failed to Validate the Version for License

Creator
Creator

Unable to find splm9.lic file in the system, where am I going wrong?

I selected 2 -tier+Corporate server for installation.

Error Failed to validate the version for license server 28000@PCxxxxx. Return value = -15 still exists