Cancel
Showing results for 
Search instead for 
Did you mean: 

Folder Access privilege : Moving a volume from server A to server B.

Valued Contributor
Valued Contributor

Thank you for reading this post.

I have some questions about Folder Access privilege.

 

I moved the volume folder from Server A to Server B.  After we finish moving the volume from Server A to Server B, the access rule of Volume folder in Server B is different from the access rule of Volume folder in Server B. I expected that because of access rule Teacemtenr cannot access to Volume folder in Server B. 

 

So my questions is : 

- To access Volume folder, Who dose teamcenter use to access volume folder such as System or Administrated user?

- When I log in to Teamcenter with UserA, not infodba and create PDF dataset, this pdf owner is UserA, right?

- After moving volume folder to Server B, Should I modify each files under Volume folder?  (I think it takes too much time...)

5 REPLIES 5

Re: Folder Access privilege : Moving a volume from server A to server B.

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The owner of the volume, and files in the volume, is the user who is running the FSC service. Lets say that you don't want "infodba" to run the FSC service so you pick another user, in my case, "ACME\Fred" is running the FSC service...
1. Change ownership of all folders/files to ACME\Fred by right-click Volumes > Properties, Security (tab) > click Advanced, Owner > click Change. Enter ACME\Fred, OK. Check "Replace all child object permission entries with inheritable permission entries from this object", OK. Close Properties.
2. Grant full control to ACME\Fred by right-click Volumes > Properties, Security (tab) > select ACME\Fred, click Edit, check Full control, Apply, click Advanced, select ACME\Fred, click Change Permissions, check "Replace all child object permission entries with inheritable permission entries from this object", OK. Close Properties.
3. Add ACME\Fred as an Author in Teamcenter. Yep, that's right, if you decide not to use the built-in account then you will consume a license for this "service" user.
4. Restart all services.

All files are written to and read from the volumes as ACME\Fred. Ownership of the Dataset object in Teamcenter is still whomever created it. But the underlying file(s) (in named references) are owned by Fred.

BTW, I don't use the built-in account on anything but Dev which is a single server. All others have a specific "service" domain level account. Why domain level? Since it needs to have the same permissions across many servers (local accounts are all unique).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: How Cadfile can be from Teamcenter 10 volume from server A to Teamcenter12 Volume of server B.

Pioneer
Pioneer

Hello Team,

i want to know the process of moving the cad files from Teamcenter10 volume from server A to Teamcenter 12 volume of Server B.

like want to understand Migration principles.

 

Regards

Sameer Kulkarni

Re: How Cadfile can be from Teamcenter 10 volume from server A to Teamcenter12 Volume of server B.

Siemens Legend Siemens Legend
Siemens Legend

there are two ways of moving files from one server to another...
#1 if you are not so experienced, create a new volume on the new server (assuming you have already a FSC installed there) and use the move_volume_files utility to move it from one server to the other
#2 if you are more experienced - just copy the files with the right OS-user (because of the access-rights on the OS-filesystem) - usually the user who drives the "Teamcenter FSC Service", and rewrite the fmsmaster-file as well as some table entries; but here you need to have really experience!
Usually I recommend the way #1 - there is not much you can do wrong there...

EDIT: I missed your header - saying you want to move it while upgrading Teamcenter - here I'd suggest consoulting your local Siemens office for assistance with that.

Re: How Cadfile can be from Teamcenter 10 volume from server A to Teamcenter12 Volume of server B.

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Uhm, move_volume_files won't work for two different environments? And its not cool to change the subject line in a post that already has a solution. Definitely two different scenarios. You should investigate csv2tcxml for migrating bulk data (fast). Or purchase a tool like IPS_Upload (no I don't sell it) which is more time consuming but might be easier to understand.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: How Cadfile can be from Teamcenter 10 volume from server A to Teamcenter12 Volume of server B.

Legend
Legend

Setting folder Access privilege  also  may need if we just copy files from one server to another, cause file security settings in server A are belong to OS user with corresponding unique GUID, on server B OS user with the same name will have different  GUID

 

But may be I'm not right