Cancel
Showing results for 
Search instead for 
Did you mean: 

Help with handler EPM-notify-report

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

I create a worflow who allows to send emails.

I receive the mail but i have an error at level of handler EPM-nofify-report if i want approve (see screen copy)

 

Thank you for your help

4 REPLIES 4

Re: Help with handler EPM-notify-report

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

What arguments are you using with EPM-notify-report? You'll need to select one of the EPM-notify-report handlers in the list (Workflow.png) in order to show the arguments.

 

I'm guessing that you're missing "-report=level" or "-report=progress" which are recommended for the Complete action where you have EPM-notify-report specified. You have two of them on Complete?


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Help with handler EPM-notify-report

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thanks for your answer.

There's the argument i've used  (See screen copy)

Re: Help with handler EPM-notify-report

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The -report switch is mandatory. -report={review|rejection|progress|level}
progress or level are acceptable for the Complete task.
https://docs.plm.automation.siemens.com/tdoc/tc/11.2.3/help/#uid:CR-notify

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Help with handler EPM-notify-report

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

It works. Thanks very much.