Cancel
Showing results for 
Search instead for 
Did you mean: 

How Import a file periodically?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi folks...
I need to import a txt file that is at a windows folder periodically... how can I do this?
I'm thinking in using WF but exists a way to import file to a dataset using WF OOTB?

4 REPLIES

Re: How Import a file periodically?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
It's not clear on which version of Teamcenter you're using but "Drag and Drop" functionality could be what you're looking for. Have you tried it yet?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: How Import a file periodically?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thanks, but I need to do this automatically... in background
drag and drop wasn't what I need

Re: How Import a file periodically?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
You can use the ips_upload utility to upload the file/s and to use the Windows scheduler to run it.

Re: How Import a file periodically?

Siemens Phenom Siemens Phenom
Siemens Phenom

If TC_ROOT and TC_DATA is available in your environment you can use plmxml_import. The password can be encrypted in a passwordfile, then run the command with option -pf. cron job or windows scheduler can be used to run the job periodically.

With some programming import can be done with Teamcenter SOA.

xtof