Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How create and view a pseudofolder

Valued Contributor
Valued Contributor

Hi everybody,

 

I request your help because, for this moment, I have not found the solutions.

 

I must create a new pseudofolder on our database and add this into your all ItemRevision.

 

I create this into BMIDE and deploy without error. bmide.bmp

 

After, I would add this into the system but in Options, I don't found BUS4_Packing.options.png

 

I would like the same like BUSCH Documents

actual.png

 

I think some people know my problem and can help me. Thank you for that.

:smileywink:

 

 

 

PLM Technical IT
6 REPLIES 6

Re: How create and view a pseudofolder

Pioneer
Pioneer

Hi

 

Are you able to create the relation in TC? If not maybe you are missing the GRM rules!?

 

BR

Frank

 

Re: How create and view a pseudofolder

Valued Contributor
Valued Contributor

I'm the admin but how do you create this relation? Can you help me?

 

BR

PLM Technical IT

Re: How create and view a pseudofolder

Pioneer
Pioneer

Hi

 

First you need to make sure that the primary object has the correct GRM Rule. You can do this in BMIDE.

 

Then you can test this by copying the secondary object and Edit->"paste special" it onto the primary object choose your relation in the popup dialog. That should create the relation.

 

If you can do this you should be able to configure your pseudofolder.

 

BR

Frank 

Re: How create and view a pseudofolder

Legend
Legend

Below are the list of steps required to create PseudoFolder

 

BMIDE

1. Create custom relation business object with required displayname (subclass of IMANRelation)

2. Add this BO as new relational property to your XXXItemRevision BO

3. Modify GRM rules of your XXXItemRevision BO. Cardinality should be 1 or above

4. Save & deploy data model

 

TC GUI

5. Login as dba and modify 2 preferences (add an entry of your custom Relation BO)

    ItemRevision_DefaultChildProperties

    ItemRevison_PseudoFolder

 

6. Clear Cache and restart TC 

 

Regards

Naveen

Re: How create and view a pseudofolder

Valued Contributor
Valued Contributor

Hi,

 

thank you for your help.

 

However, I haven't to do change with GRM Rules. That is possible, my database is already configure by default for a pseudofolder?

 

Regards

PLM Technical IT

Re: How create and view a pseudofolder

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

As was mentioned, you have to (in BMIDE):

1) add BUS4_Packing as a relation property under your "DEV Revision" business object.

2) modify the GRM rules for your "DEV Revision" business object to define cardinality for the BUS4_Packing relation.

 

Then in the rich client:

3) modify the DEVRevision_DefaultChildProperties preference to include the BUS4_Packing relation, and 

4) modify the DEVRevison_PseudoFolder preference to include the BUS4_Packing relation.

 

The first preference makes objects attached to your "DEV Revision" visible to your users and the second makes the relation appear as a pseudofolder. Make sure you make the modifications as a dba and the preferences' scope are both SITE.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC