Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Dear all 

      My sofeware version is TC11.5.3 & TC 11.6 ; I want to add a new property for TC_Project ;

  1.       I was created a new property for TC_Project in BMIDE;
  2.       It was deployed successfully. I can see and modify this property with existing projects  in 4-Tier Rich Client; 
  3.       When I want to create a new project, the system reminds me that there are empty properties, and create a failure;
  4.       After that , I removed this  property in BMIDE and deploy again ; At this time , I can create a new project successfully without the property;

     So, How can I do if I want to add a new prperty for TC_Project this object ?

 

 

 

9 REPLIES 9

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

You have to set an initial value (in BMIDE) for the TC_Project custom property.

I used - for string properties.

Tricia Crichton | Software Architect | SEAL PLM, Inc

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks for your reply !!

          As you said,I should set an initial value (in BMIDE) for the TC_Project custom property.

          Not only the initial value , but also not null ;

Re: How to add a new property for TC_Project in BMIDE ?

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon @wrun , I think the answer @TCrichton  also deserved a mark as a solution

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Good afternoon @ArthurRM , you are right !

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi,wrun,i also created a new property for TC_Project in BMIDE,but after deploying,i can not see it in TC_Project in RAC.
Is there any other configurations?BTW,based on TC11.5.
Thans a lot!

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi @ydxxzjican 

    You should set an initial value (in BMIDE) for the TC_Project custom property.

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,@wrun Sorry for the late reply. As you suggested,i set an initial value (in BMIDE) for the TC_Project custom property ,however ,still does not work. I can not see it in TC_Project in RAC.But i can find the property by print it. Is there any other configurations i missed?Thans a lot!

微信截图_20190807135657.png微信截图_20190807135739.png

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

hi @ydxxzjican 

      Maybe you can try to clear the client cache.

Re: How to add a new property for TC_Project in BMIDE ?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks for your quick reply !And it still does not work.