Cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure and launch NX with embedded AWC

Pioneer
Pioneer

Hi Team

 

We have installed Teamcenter 12.1, AWC 4.1.4 and NX 12.0.2. Could you please let me know how to configure and launch NX with embedded AWC.

Thanks & Regards

Harish

7 REPLIES 7

Re: How to configure and launch NX with embedded AWC

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, you need to set values for the following parameters:

 

Setting up Active Workspace embedded in NX
https://docs.plm.automation.siemens.com/tdoc/nx/12.0.2/nx_help/#uid:xid814861

Betreff: How to configure and launch NX with embedded AWC

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Make a copy of your %TC_ROOT%\portal\start_nxmanager.bat

Name it eg. start_nxmanager_managed.bat

open it in editor.

modify the following lines:   

...

set NTIER_ARG=4-tier

...

:4-tier
rem set the communication mode
set UGII_UGMGR_COMMUNICATION=HTTP
set UGII_UGMGR_HTTP_URL=http://[hostname]:[port]/tc/aiws/aiwebservice

 

The preference ActiveWorkspaceHosting.NX.URL should be set as well.

 

run the start_nxmanager_managed.bat

Michael
Teamcenter UA | NX CAD

Betreff: How to configure and launch NX with embedded AWC

Pioneer
Pioneer

Hi Arthur and Michael

 

Thanks for the response.

 

@Michael_Ruhnke 

 

We will provide only Activeworkspace URL to user machines and we will not provide rich client.Could you please let me know you are saying to edit in server or in user machines rich client %TC_ROOT%\portal\start_nxmanager.bat.

 

In user machine there should be only Active workspace URL and NX and no rich client.

 

Thanks & Rergards

Harish

Betreff: How to configure and launch NX with embedded AWC

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

The modified start_nxmanager.bat should be available on every user client.

Michael
Teamcenter UA | NX CAD

Betreff: How to configure and launch NX with embedded AWC

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
@Harishkumar, you should adjust your thinking for this solution. It looks like you're thinking that AWC is a zero install therefore nothing should have to be installed on the client. However, you are asking about embedded AWC which resides inside NX and is launched when NX is launched. NX is installed on the client.

The solution from @Michael_Ruhnke is launching Managed NX. The solution from @ArthurRM is launching Native NX with embedded AWC. Either solution works. Debugging...
https://docs.plm.automation.siemens.com/tdoc/nx/12.0.2/nx_help#uid:index_tcint:xid859791:xid922781

@Harishkumar, do you already use NX Custom for setting NX site preferences without modifying each users NX installation on their workstation? If not then you may want to look at it since it allows a single network location.
https://community.plm.automation.siemens.com/t5/NX-Programming-Customization-Forum/NXcustom-Utilitie...

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Betreff: How to configure and launch NX with embedded AWC

Pioneer
Pioneer

Hi Michael and Randy

 

Thanks for the help.I have configured with respect to document and under NX resource bar, I can able to see AWC icon but when I am clicking on AWC icon, it showing error as "Internal Memory access violation" and "index out of range" error.Please find attached image. 

 

From the AWC, I can able to open NX by selecting existing NX data and clicking on "open in NX" command.But, when clicking on AWC icon on NX resource bar, I am getting this "index out of range error".

 

Thanks & Regards

Harish

Betreff: How to configure and launch NX with embedded AWC

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Looks like you're missing a required MSVS redistributable for running AWC. Check the install docs for the exact ones you need.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4