Cancel
Showing results for 
Search instead for 
Did you mean: 

How to delete a PBO when project not available in BMIDE

Legend
Legend

Good afternoon,

I created a PBO with BMIDE and deployed the template to Teamcenter, after that, the project was corrupted and deleted. Now I cannot delete the PBO from Teamcenter and it is offering it when 'new item' is selected. Any ideas about how should I proceed to remove it completely from TC? Is it possible to do from the command line? from the GUI as infodba?

 

Thank you.

5 REPLIES 5

Re: How to delete a PBO when project not available in BMIDE

Phenom
Phenom
you can try to build a BMIDE package manually using installed files from following locations and then install the updated template again.

1. Feature XML:
%TC_ROOT%\install\install\modules\feature_<templateName>.xml
2. lang, properties and default files:
%TC_ROOT%\install\<templateName>\
3. template.xml and dependency.xml from
%TC_DATA%\model\

Re: How to delete a PBO when project not available in BMIDE

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can recreate the project by importing it from a package. Go to File -> Import,

 

File-Import-FromPackage.png

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC
Highlighted

Re: How to delete a PBO when project not available in BMIDE

Legend
Legend

Thank you!

Re: How to delete a PBO when project not available in BMIDE

Legend
Legend
Thank you!

Re: How to delete a PBO when project not available in BMIDE

Legend
Legend

In fact it was very easy to achieve. I just recreated an empty project with the same name and pefix, created the target class, deployed it and then redeployed it after deleting the PBO from the project. It did work fine.

 

Thank you both for your quick replies.