Cancel
Showing results for 
Search instead for 
Did you mean: 

How to find value of PropertyDescriptor using SOA API ?

Experimenter
Experimenter

Within the field 'SoaType' of a Form there is a subfield 'PropDescs' which contains the names of fields on the form, but not the values.

 

For ex. the field 'owning_group' contains the key 'owning_group' and the value '{Teamcenter.Soa.Internal.Client.Model.PropertyDescriptionImpl}', not the string containing the owning_group's name.

 

Rather the value exposes the PropertyDescription type members, ex. 'enabled, FieldType, InitialValue, Localizable, LovCategory' to name a few, but again, the actual value within the field is not present/or loaded.

 

Running DataManagementService.GetProperties on the WorkspaceObject representing the Form is not loading any additional properties, namely, Object_properties which appears to be the field desired in this case.

 

GetAttachedPropDescs2 documentation wording isn't providing clarity - "Get the attached property descriptor based on input type name and property names structure."

 

Is this meaning it takes an input type, ex. "ItemRevision", and ex. name "object_name", that the output would be "String" or the actual value stored in object_name?

 

Similarly, how does this method know which object to pull the data from?

 

tl;dr - How to load the entered value for a given field on a form and retrieve it?

1 REPLY

Re: How to find value of PropertyDescriptor using SOA API ?

Experimenter
Experimenter

ModelObject.GetProperty(string propertyName) returns an 'Properpty' object which contains the data in a variety of parameters. 'DisplayValue', 'StringValue', et cetera.

 

Edit: to include an example.

 

Note: this returns custom properties created via the BMIDE as well, at least, for me.

ex: 

// Load the property
Teamcenter.Soa.Client.Model.Property temp = ModelObject.GetProperty("owning_user");

// Data entered into "owning_user" field
string refFormText = temp.StringValue;