Cancel
Showing results for 
Search instead for 
Did you mean: 

How to install NX integration with TEM with command line parameters

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For NX 10 the NX integration feature of TEM is mandatory, so we need to add it to about 100 machines.

We are deploying Teamcenter through TEM silently, which works quite good.

Starting with Tc 10.1.4 TEM also supports the feature argument to add single features, so we would like to use that.

So what would be the correct command line to add the feature Teamcenter Integration for NX to an existing Tc client installation?

The documentation is not really clear about this, so find my proposal below.

tem -install -features="Teamcenter Integration for NX"

Thanks in advance for any pointers into the right direction.

 

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
3 REPLIES

Re: How to install NX integration with TEM with command line parameters

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Try:

tem -u=<username> -p=<password> -install -features "750315D3BEB2810D3A4FA698D8EAED8A" -showscript

Instead of figuring this command-line syntax out, it might be easier to use TEM and the "Create Silent Distribution" option and then use the result in a batch file to roll out the new feature to your clients:

tem -s <the silent XML file>

 

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: How to install NX integration with TEM with command line parameters

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks Arden, I will try the proposed syntax and report back.

We do install on a blank system and update to a patch level using TEM with the silent switch, but I have never tried to add features with this approach. Do you have had success doing this in the past? I can't effort damaging a bunch of our systems, it is too cumbersome to reinstall on more than a hand full of systems.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: How to install NX integration with TEM with command line parameters

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Adding the feature through the command line parameters resulted in a failed installation.

Will have to check my other options.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide