Cancel
Showing results for 
Search instead for 
Did you mean: 

How to restrict users to open Native NX and force to use TC Integrated NX always?

Genius
Genius

Is there a setting or configuration to force the users to use TC Integrated NX (Managed Mode) Not Native NX ?

 

 Any thoughts or pointers would be highly appreciated.

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |
1 REPLY 1

Re: How to restrict users to open Native NX and force to use TC Integrated NX always?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
I've tried hiding/removing the NX icons in C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Siemens NX 11.0\ however users are creative and will always find a way. The only thing that works is an edict and enforcement from upper management with repercussions if "standards" are not followed. Make sure to outline all the use-cases where native is appropriate and make clear that only those cases are allowed.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4