Cancel
Showing results for 
Search instead for 
Did you mean: 

How to set Timeout duration for AWC 3.1 client?

Valued Contributor
Valued Contributor

How do I set the timeout duration for AWC clients? 

 

If working in web client it is not a big deal to re-login, but if working in NX managed mode with AWC then it seems like i have to restart the whole NX managed session if awc is timing out. 

 

4 REPLIES 4

Re: How to set Timeout duration for AWC 3.1 client?

Siemens Phenom Siemens Phenom
Siemens Phenom

If you increase the session time out it affects RAC, thin client, and AWC. There is no extra time out for AWC. I think per default it is 30 min.

xtof

Re: How to set Timeout duration for AWC 3.1 client?

Valued Contributor
Valued Contributor

Hi

 

Thanks for quick reply. 

 

So in a .net environment, it would be this value that will cause timeout?

Spoiler

Soft Time Out Stateless

(Optional) Specifies the time-out for stateless mode servers in a busy pool in seconds. The default value is 1200.

timeout.jpg

 

Brgds, 

 

ØK

Re: How to set Timeout duration for AWC 3.1 client?

Siemens Phenom Siemens Phenom
Siemens Phenom

yes, this is the time out for stateless servers if the pool is above target.

I would not change these values in a productive enviroment without a good understanding of their relations and their impact on performance.

 

xtof

Re: How to set Timeout duration for AWC 3.1 client?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

One can set it from TC Pool Manager Global Configuration. Check below image for reference.
Untitled.jpg