Cancel
Showing results for 
Search instead for 
Did you mean: 

How to update String Arry property value using SOA?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I have property with type String Array. Using SOA how to update the
value?


Owen
Regards

2 REPLIES 2

Re: How to update String Arry property value using SOA?

DataManagementService.setProperties( ) can be used. Need to pass, object as 1st argument and 2nd argument (which is map by the way) can contain property names and property value (or list of property values). 

Re: How to update String Arry property value using SOA?

Phenom
Phenom

Using DataManagementService.SetCustomProperties() you can provide NameValueStruct with Values as String array.

If the property is an array, then all provided values are updated, if property is not an array, only the first value is considered.