Cancel
Showing results for 
Search instead for 
Did you mean: 

Identify the type of NX file (Component/Assembly/Drawing)

Builder
Builder

Hello Experts,

 

NX data is managed in teamcenter. Under an item-revision i have multiple UG datasets only one of them is a "UGMaster" the rest of them are "UGPART". I need to differentiate which one of them is a component/assembly/drawing. Below is an example from teamcenter. The ones boxed in "RED" are UG/NX datasets.

 

Item_Sample.PNG

 

 

 

 

 

 

 

 

 

 

 

 

 

Any help or suggestions would be helpful. 

Regards,
Santosh
2 REPLIES 2

Re: Identify the type of NX file (Component/Assembly/Drawing)

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @santosh0114,

With master model approach

UGMASTER - 3D geometry

UGPART - Drawing

 

UGMASTER can represent a piece part or an assembly. As item has BVR so that UGMASTER should be an assembly.

Re: Identify the type of NX file (Component/Assembly/Drawing)

Builder
Builder

Hi @GaneshKadole

 

I agree and that was my first approach.

 

There is a possibility that the user might have checked in an peice part (3D Geometry) as UGPart. I am trying to figure this one out.

Regards,
Santosh