Cancel
Showing results for 
Search instead for 
Did you mean: 

Import XMLRenderingStylesheet

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

Our customer has TCRS with Solid Edge,  but because it is more civil engineering branch, they still need to work with Autocad. But the version is Autocad LT and we could not employ autocad integration. We want at least for them to be able to open dwg file from Teamcenter. At closing of dwg file the Dataset Open/Open window error will appear: Unable to import file C:\......Drawing1.dwl, Details: No file template is defined for file with extension .dwl

I know that these file are temporary created by Autocad. But is there any hint how to fix this in Teamcenter (some workaround)?

3 REPLIES 3

Re: Import XMLRenderingStylesheet

Siemens Genius Siemens Genius
Siemens Genius

Consider saving the Autocad drawings in DWG ot PDF format and import these files to Teamcenter.

Will that not solve your issue?

 

Kind regards,

Arun Kumar G

Autocad file in Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

it is not problem to import dwg file.

I need that the user is able to open the file by doubleclick (this works), can edit it and save. At saving there is that arror.

Re: Autocad file in Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Meanwhile the problem has been solved - this is only a issue of AutoCAD version 15. Versions 16 and 17 works good.

So the solution is to upgrade AutoCAD.