04-05-2018 05:05 AM
Hi.
I'm doing a Thesis work at a company which uses Teamcenter and NX. The work started out with creating some company specific custom checkers for check-mate and now I'm looking on how do do a good teamcenter integration for these. I've also created a rule set with the Validation Rule Editor to use and tried this in NX (without TC) and it works fine.
Now I want to import this rule set file into teamcenter to have it work there as well and after this design workflows that demand some rulesets in order to proceed.
I dont know how to import this rule set file into teamcenter however. I do have the dba role!
Regards Emil
04-05-2018 07:54 AM
Good afternoon, I do not have much experience with Check Mate, but I'll try to help where you can find information.
Do you have access to the Teamcenter and NX help? If so, find and read the Validation Manager Guide
Also, in the NX Help, see the following section:
04-05-2018 08:44 AM
Thank you. I do have acess to NX help. It seems it wants some log in details from me when I want to use the Teamcenter Help.
I must ask my supervisor about a user for this or if there are insall files somewhere for this.
04-05-2018 10:02 AM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4