Cancel
Showing results for 
Search instead for 
Did you mean: 

Importing pax files to create Pallettes for users

Experimenter
Experimenter

I have pax files that I have created outside of TCe.  They have been formatted to be able to be imported into TCe.  I now need to know how and where to import them into TCe so they can be used for pallettes.  I also want the pallettes to show up for all of the NX users.  Any help would be appreciated.

 

Thanks

Jeff

1 REPLY

Re: Importing pax files to create Pallettes for users

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

See the sample script in UGII_BASE_DIR\UGII\templates\sample\tcin_template_setup.bat

 

1. Copy the script to UGII_BASE_DIR\UGII\templates

 

2. Start a Teamcenter command prompt then run:

cd %UGII_BASE_DIR%\UGII\templates

tcin_template_setup.bat -u=infodba -p=infodba -g=dba

 

This tool will import the templates by launching nx_clone in managed mode.

 

Note: you'll get a new revision for existing Items in Teamcenter. If that's not what you want then you can overwrite existing files using the "-a=overwrite" switch.

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2