Cancel
Showing results for 
Search instead for 
Did you mean: 

Initial value display incorrectly

Experimenter
Experimenter

Hi,

 

I have custom attribute which has inital value set. Attribute is used when creating "Change Notice". Attribute has also "Batch LOV" attached.

 

Probelm is that initial value does not show correctly on when creating "Change Notice". If i detach "Batch LOV" from attribute initial value is displayed correctly. I have attached picture from problem

 

Teamcenter:

Teamcenter 10 (10.1.3(20141202.00)) 64-bit 

4 REPLIES

Re: Initial value display incorrectly

Legend
Legend

Does your initial value exist in LOV (exactly same) ?

Re: Initial value display incorrectly

Experimenter
Experimenter

Yes it does and i tried with several values as well.

 

I don't know if this has nothing to do with the problem but there's renderingHint="lovuicomp" used in stylesheet with problematic attribute.

 

If i remove renderingHint, default value is displayed correctly but the the field dosen't behave like it should be

Re: Initial value display incorrectly

Pioneer
Pioneer
The LOV Entries are completely localized?
( In case of more than one language : There is a localization value assigned for every language, even If its the same value for different languagaes? )
Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX11.0.2.7 MP04 + TC10.1.7.1
Testing: NX11.0.2.7 MP11 + TC10.1.7.1
Unstable: NX12.0.2.9 MP02 + TC11.5.0.2
Development: C#

Re: Initial value display incorrectly

Experimenter
Experimenter

Yes LOV is localized as en_us language. This localized lov is in different file which has same list of values as TcLOV has