Cancel
Showing results for 
Search instead for 
Did you mean: 

Installing TC 10.1.3 directly with a compact distribution

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

I installed TC Rapid Start 10.1 and patched it to 10.1.3 on corporate server and next week I'll install 7 Rich Clients.

 

Which would be the fastest way?

I want to create a compact distribution with 10.1.3 and install all the clients this way.

Is this possible? And how?

 

Cem

14 REPLIES

Re: Installing TC 10.1.3 directly with a compact distribution

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can record a silent installation when you start the TEM of 10.1.3, which will also include installing the base release.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Installing TC 10.1.3 directly with a compact distribution

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Stefan,

 

Actually, what I want to achieve is to create a custom distribution file.

When I start TEM on a 10.1.3 Rich Client, this option is not available.

1.jpg

 

When I start tem.bat from the distribution image of 10.1, I see this option

1.jpg

1.jpg

 

But in this case I think only 10.1 files will be inside and I will need to patch again.

 

And If I create a silent.xml from 10.1.3 rich client, with which distribution image will I use it with? I have 10.1 and 10.1.3 patch 

 

Cem

 

Re: Installing TC 10.1.3 directly with a compact distribution

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The silent installation through 10.1.3 will need both, the base and the patch distribution.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Installing TC 10.1.3 directly with a compact distribution

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

TcRS 10.1.3 is not a super kit like Teamcenter 10.1.3, that is why 'compact distribution' option is disable. With TcRS we started super kit concept from patch 10.1.4 onwards. For TcRS 10.1.3 use the silent installation method.

 

Re: Installing TC 10.1.3 directly with a compact distribution

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Then I go and download 10.1.4 directly Smiley Happy

Re: Installing TC 10.1.3 directly with a compact distribution

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

So Ravi,

 

Can we install TcRS with 10.1.4 directly without installing 10.1.0 base?

 

Cem

Re: Installing TC 10.1.3 directly with a compact distribution

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The short answer is no. You'll need both Tc10.1.0 and Tc10.1.4 for the Super Kit method. Start by launching the media TEM from Tc10.1.4 then when prompted for the "Original Media Location", enter the path to the Tc10.1.0 media (for instance C:\Temp\Tc10.1.0_win64. The "Update Location" will contain any/all patches. The path to the Tc10.1.4 media will be automatically added since it was used to launch TEM.

 

If you had more than one patch, like Tc10.1.4.1, then you would:

1. Run the media TEM from the latest patch.

2. Specify the location of the original media (example: C:\Temp\Tc10.1.0_win64).

3. The update location list will already contain C:\Temp\Tc10.1.4_patch_1_wntx64\wntx64.

4. Browse to intermediary patch (example: C:\Temp\Tc10.1.4_wntx64\wntx64).

5. Move the intermediary patch up in the list (Shift Up).

 

Final order will look like:

C:\Temp\Tc10.1.0_win64

C:\Temp\Tc10.1.4_wntx64\wntx64

C:\Temp\Tc10.1.4_patch_1_wntx64\wntx64

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Installing TC 10.1.3 directly with a compact distribution

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Thanks for detail explanation Randy

-Ravi

Re: Installing TC 10.1.3 directly with a compact distribution

Legend
Legend

Hi

 

I have the same in TC10.1.4 maintenace pack that I'm not able to select the 'create compact deployable media'.

I'm using TC unified and not using RapidStart.

 

Did it work for you CemAlpay and has someone elese got it to work on an non RS setup?