Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Integration of Teamcenter 12 and Creo 5

Experimenter
Experimenter

I am using Creo 5. I want to integrate Creo 5 to Teamcenter 12.  I  will be using TC 12 for the first time. Please guide me what are the exact requirements of this integration. Is Teamcenter 12 enough for integration with Creo 5 or I need some additional software?

4 REPLIES 4

Re: Integration of Teamcenter 12 and Creo 5

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, I think you need to download from GTAC last version "Teamcenter integration for Creo", there you will also find documentation which you can read.
I'm not sure about the integration of the latest versions of Creo 5 and Teamcenter 12, you may have to contact GTAC to clarify this issue.
There is also a good specialist at the community RandyEllsworth, maybe he can answer you something on this issue.

Re: Integration of Teamcenter 12 and Creo 5

Genius
Genius

@israr_69 @ArthurRM

Hello;

Creo connector for TC12 in not yet published.

 

BR.

Re: Integration of Teamcenter 12 and Creo 5

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Creo 5 is not supported for Tc12 (yet?). Further, IPEM isn't available for Tc12 as @JFK1963 stated. However, there likely isn't much difference between IPEM 11.5 (actually use 11.5.1) and 12 so you might be able to get away with it. You would likely need to use Deployment Center so download "Teamcenter_Integration_for_Creo_11.5.0_DCTemplates.zip". And you will likely want the JT translator PLM_Components_JT_Translator_for_CREO4_CREO5_v14_0_64Bit.7z
https://download.industrysoftware.automation.siemens.com/download-n.php/tcvis/full_products/JT_Trans...

Likely, Creo 5 is your biggest challenge. Maybe @PeterH (Peter Heath) from ITI can chime in?

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Integration of Teamcenter 12 and Creo 5

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Lorraine Dennis from ITI. 

Creo 5 and Teamcenter 12 are both supported starting with Teamcenter Integration for Creo (ipem) for version 11.5.1. Capture.JPGSnapshot of the read me file

 The Readme file is also attached.