Cancel
Showing results for 
Search instead for 
Did you mean: 

Intelligent Part Numbering in CAD with ITK?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

We don't have IPN or SmartCodes available in NX (yet?), but it should be possible with customization. Has anyone actually done this? Which ITK classes/methods would be applicable?

1 REPLY

Re: Intelligent Part Numbering in CAD with ITK?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
I used to do this kind of thing in USER_part_no.c which is in the samples directory for TC. If you can't find the samples directory then you'll need to install that feature in TEM. I'm not sure that USER_part_no.c is valid anymore even though its in samples so check with GTAC before going off the deep end.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4