11-30-2018 03:13 AM
How can I build Interdependent LOV with three 3 level?
- Level1 The user first selects a material group
- Level2 The user selects a material sub group. The options should be filtered / restricted based on the selection in level 1
- Level3 The user should be able select up to 4 products (so 4 LOV fields) . The options should be filtered/restricted based on the material sub group.
The target is to increase the data quality. Today the user can any combination. Even if the product belongs to a different material sub group.
I'm currently using TC 11.2
Is it corrent that TC supports Interdependent LOV with 2 level only?
Cheers
11-30-2018 04:30 PM
TC11 allows for more than 2 levels of interdependent lov's. Each level has to be balanced and that is what makes this difficult. An interdependent lov is setting a property value for each level, there must be an lov attached for each level or the BMIDE won't let you create it. Once you have all levels defined it will work. But maybe a dynamic lov might be a better choice?