Cancel
Showing results for 
Search instead for 
Did you mean: 

Is Whole file cache and segment cache configuration mutually exclusive?

Genius
Genius

Hi Experts,

 

In a Teamcenter environment, segment cache is configured for FSC cache. As per a new requirement to load large cache, Switching to whole file cache was suggested. In this context i am looking for few clarifications. Request your help.

 

1. As per documentation, if we set the below, whole file cache gets enabled. Does that mean segment cache gets disabled?

<property name="FSC_FilesPerWholeFileCacheDir" value="1" overridable="true" />

2. Does it makes sense to set segment cache values(Read/Write) when whole file cache is enabled?

3. Is there any recommendation to have specific values/Limits for segment cache when whole file cache is enabled?

 

Thanks

Phani

2 REPLIES 2

Re: Is Whole file cache and segment cache configuration mutually exclusive?

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
A Segment Cache needs to be tuned using the spreadsheet in FSC_HOME\bin. A Segment Cache is required for streaming files (like JT's). A Whole File Cache (WFC) does not need to be tuned but the size needs to be defined. FSC's are smart and will use whichever mechanism needed to transfer files. Some companies will install multiple FSC's on the same server for different purposes like one for WFC and the second for Segment for performance reasons while other companies will install a single FSC and let FMS sort it out. Your mileage may vary.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Is Whole file cache and segment cache configuration mutually exclusive?

Genius
Genius

Thanks for the inputs Randy.

Will proceed with single FSC having both segment and wholefile cache and check the performance.

 

Thanks

Phani