Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Re: Is there any other way to install OTW client with out using Browser

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor

Of course, I have several custom ICD's that I use. One is for adding NX custom to the integration for NX solution (modifies start_nxmanager.bat). Another is for the basic install to support multiple clients on the same workstation (modifies otwportal.bat). Another is for deploying custom status icons (adds files to plugins dir). Etc.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Is there any other way to install OTW client with out using Browser

Genius
Genius

Thanks all for your valuable inputs.

 

seems I got the one i am looking for.

I have shared the webapp_root folder of distribution Instance.

Placed supporting JRE7 folder inside webapp_root.

 

--JRE7
--jtutilities
--otwweb
|- otw.bat (Added manually inside otwweb)
|- otwinstaller.properties (Added manually inside otwweb)
--wntx64
--otw_installer.jar
--otw_installer.zip

 

otw.bat contains:

"..\jre7\bin\javaw.exe" -cp otw_installer.jar com.teamcenter.install.otw.installer.Installer

 

otwinstaller.properties contains

instance=DEV_Instance
server_name=SERVERNAME.DOMAIN\:12095
Silent=
logging=FINE

 

mapped the shared webapp_root folder, set JRE64_HOME to JRE7 folder inside webapp_root and called otw.bat in a command shell.

Able to install the same OTW without using browser. war file deployment is also not needed for this way of installation.

 

Thanks
Phani

Re: Is there any other way to install OTW client with out using Browser

Experimenter
Experimenter

Hi Phani,

 

I tried this method, but the installer is not proceeding, it is showing 0%..... and struck.

Any Idea.

Re: Is there any other way to install OTW client with out using Browser

Experimenter
Experimenter

Got it resolved by adding commons-lang and jdom jars

 

otw_installer.jar;commons-lang.jar;jdom.jar