Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any other way to install OTW client with out using Browser

Genius
Genius

Hi,

 

Recently we upgraded teamcenter client and facing issues in puching OTW client, with browser issues.

Please suggest any workaround to install with out using browser and its associated plugins

 

Thanks

Phani

13 REPLIES 13

Re: Is there any other way to install OTW client with out using Browser

Phenom
Phenom

you can install 4Tier client using tem.bat. Select only one option "Rich Client 4 Tier" on Solutions page.

Re: Is there any other way to install OTW client with out using Browser

Phenom
Phenom

Here is a doc for TC10  4Tier RAC installation with screenshots which I prepared for my colleagues.

Re: Is there any other way to install OTW client with out using Browser

Genius
Genius

Thanks a lot for the detailed documentation.

 

I am looking to distribute the OTW client (find it easy to push the updates)only without using browser

Re: Is there any other way to install OTW client with out using Browser

Experimenter
Experimenter
What are the issues during the upgrade. We use OTW since 2005 and it seems that we are already faced with all of them.

Re: Is there any other way to install OTW client with out using Browser

Genius
Genius

Java plugin issue in IE11. even though latest java is installed explorer is not picking up

Re: Is there any other way to install OTW client with out using Browser

Siemens Phenom Siemens Phenom
Siemens Phenom

Come to my presentation, Deploying Clients Via Windows Batch Scripting, at this month's PLM World Conference in Orlando where I walk through this very process in detail. 


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Is there any other way to install OTW client with out using Browser

Experimenter
Experimenter

There is a little trick if you use IE 9 and higher and your OS Windows is x64

 

 

http://answers.microsoft.com/en-us/ie/forum/ie10-windows_8/java-plugin-for-internet-explorer-x64-not...

 

Proposed Solution:

  1. Install x64 JRE or JDK
  2. Open registry editor and set the following value to 0

HKEY_CURRENT_USER\Software\Microsoft\Internet Explorer\Main\TabProcGrowth

If it doesn't exist, then create the entry as a DWORD

 

Now all the pages will run as x64, even those that use Java or Flash.

 

This solution worked, was able to recognize JDK and I was able to utilize the OTW Client with IE 10

 

P.S. system or user environment preference JRE64_HOME must be set.

P.P.S. And you should run IE by clicking RMB and choising Run as Administrator

Re: Is there any other way to install OTW client with out using Browser

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

There is a way, but it depends on the solutions you choose. This is OTW so you'll need to install the first client using a browser (doesn't have to be IE11).

  1. Install the OTW rich client on workstation 1.
  2. Zip the contents of the installed client on workstation 1.
  3. Copy and unzip the client on workstation N.

The NX integration will not have the registry setting for start_nxmanager.bat so you'll need to set it after unzipping the client. Teamcenter Visualization (Embedded) will make a whole lot of registry entries so do not use this method if you're selecting any TcVis solutions. Other solutions, especially the integrations, probably make registry entries also and should either be recorded and duplicated or avoided altogether. If you require integrations then use an alternate method like a TEM silent install that Larry discussed.

 


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Is there any other way to install OTW client with out using Browser

Experimenter
Experimenter
It is possible to make changes (add, remove or replace lines) into the bat-files via icd-file (OTW) for configuring integrations.