Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any way to input ® symbol in property

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi All!

Is there any way to input ® symbol which means registered trademark in Teamcenter?

Thanks a lot!

5 REPLIES 5

Re: Is there any way to input ® symbol in property

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
The ASCII code for Registered Trademark is ALT+0174 (number pad) however not all computers support it and an approximation is normally used instead (R).

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Is there any way to input ® symbol in property

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Appreciate your reply Randy!Using a computer has separate number panel, i can input the symbol in ‘Edit Properties’ panel by the way you provided (It does not work In Summary Page).However, the symbol changes to "?" when i check-in and database displays same symbol.It seems to about DB Character set or encoding.

Re: Is there any way to input ® symbol in property

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

It should work in a standard ANSI teamcenter environment. I'm able to store the ® in an attribute in property window, in an attribute in summary view or as LOV value in BMIDE.

 

SQL DB encoding is Latin1_General_BIN (default).

RAC character encoding is ISO8859_1

BMIDE TextServer encoding is ISO8859_1/ISO8859_2

XML Stylesheets are UTF-8 by default

property font depends on windows font setting

 

Check your TC_language_* preference variables on encoding mismatch.

Michael
Teamcenter UA | NX CAD

Re: Is there any way to input ® symbol in property

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Sorry for the late reply Michael! I'm using Oracle Database.I have checked preference variables you mentioned and find nothing.

Re: Is there any way to input ® symbol in property

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

To see these language preferences, choose Edit →Options, click the Filters or Search at the bottom of the Options dialog box, and search for preferences beginning with TC_language.

I guess the Preference 'TC_language_default' is available only in a localized environment.

 

TC_language.png

Michael
Teamcenter UA | NX CAD