Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Issue Management in Teamcenter

Genius
Genius

I have couple of questions on Issue Management in Teamcenter. Was wondering if some one could answer these.

 

1) Is Issue Management in Teamcenter is separte from Issue Management and CAPA in Technomatix ?

 

2) Can the standard OOTB Teamcenter issue management be configured to use in the Active Workspace ?

 

Any references / documents / pointers would be highly appreciated.

 

Thanks,

TCNinja.

 

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |
2 REPLIES 2

Re: Issue Management in Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I can help with question 1: Teamcenter Issue Manager is different and separate from Issue Management and CAPA.  Teamcenter Issue Manager is installed using TEM and is closely aligned with Teamcenter Change Management, while Issue Management and CAPA provides a bespoke web UI that offers a quality-focused method for addressing issues.

 

-Patrick

 

Patrick (Pat) Kennedy, Sr. PLM Application Engineer, Acuity Solutions

Re: Issue Management in Teamcenter

Genius
Genius

Thanks Patrick,

 

 

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |