Cancel
Showing results for 
Search instead for 
Did you mean: 

Issues when upgrading from TC server 10 to TC server 11.2.0

Experimenter
Experimenter


I tried to upgrade the TeamCenter server from version 10.1 to version 11.2.0 on XenCenter Virtual Machine with the OS "SUSE Linux-64, openSUSE 11.4"
I used the archives Tc11.2.0_lnx64_1_of_2.zip and Tc11.2.0_lnx64_2_of_2.zip
First of all, I verified that the software requirements are met:
The JRE version is 1.7.0_45.
The DataBase is Oracle Database 11g Enterprise Edition Release 11.2.0.1.0 - 64bit Production.
The upgrade stops with the error below (contained in the file install_MYDB_1611211859.txt from the attached archive errors_upgrade_TC_11.2.0.zip). The error is:


----------------------------------------------------------------------------
Executing command 26 of 149...
Section: schema-add
File: upgrade_runner
Command: business_model_updater -u=infodba -p=${TC_USER_PASSWD} -g=dba -mode=upgrade -update=schema_revisability_option -process=change -file=/opt/tc/teamcenterdata2/model/delta.xml
----------------------------------------------------------------------------
Command start time: Mon Nov 21 07:05:11 PM 2016
Output:


Command end time: Mon Nov 21 07:05:14 PM 2016
Command duration: 3.574 seconds
ERROR: Execution of command 26 failed


----------------------------------------------------------------------------
Executing command 26 of 149...
Section: schema-add
File: upgrade_runner
Command: business_model_updater -u=infodba -p=${TC_USER_PASSWD} -g=dba -mode=upgrade -update=schema_revisability_option -process=change -file=/opt/tc/teamcenterdata2/model/delta.xml
----------------------------------------------------------------------------
Command start time: Mon Nov 21 07:05:14 PM 2016
Output:


Command end time: Mon Nov 21 07:05:18 PM 2016
Command duration: 3.629 seconds
ERROR: Execution of command 26 failed

Upgrade end time: Mon Nov 21 07:05:18 PM 2016
Upgrade duration: 1 minutes 21.509 seconds
ERROR: Upgrade failed.
command_exit=215
Exit Status  215, elapsed time 0:01:24
Command upgrade_runner has failed with status 215
Checking for existence of '/opt/tc/Siemens/Teamcenter11_3/install/upgrade_display_results.log'
Opening '/opt/tc/Siemens/Teamcenter11_3/install/upgrade_display_results.log' for reading.
Begin parsing: Mon Nov 21 19:05:20 CET 2016
Parsing complete: Mon Nov 21 19:05:20 CET 2016
'/opt/tc/Siemens/Teamcenter11_3/install/upgrade_display_results.log' was successfully parsed....1 comment(s) added to the comment store
Capturing related logs and information available: Mon Nov 21 19:05:20 CET 2016
Generating list of the latest logs
List of logs generated...list contains 1 log(s)
Adding installation log to the list of related logs
Attempting to access latest version of '/opt/tc/Siemens/Teamcenter11_3/install'
Latest version available: /opt/tc/Siemens/Teamcenter11_3/install/install_MYDB_1611211859.log
Converting list of logs to an array
Accessing the comment store
Comment store opened...accessing comments
Adding 1 comment(s) to exception list
Releasing the command shell
Generating exception: Mon Nov 21 19:05:22 CET 2016
An error occurred during execution.  Stack trace follows...
com.teamcenter.install.tceng.base.DatabaseSteps.upgradeDatabase(DatabaseSteps.java:944)
com.teamcenter.install.tceng.base.Foundation.install(Foundation.java:185)
com.teamcenter.install.tceng.base.Foundation.upgrade(Foundation.java:1134)
sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:57)
sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
java.lang.reflect.Method.invoke(Method.java:606)
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:209)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:128)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:201)
com.teamcenter.install.tem.struct.TcFeature.processAction(TcFeature.java:1407)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1345)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1245)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1159)
com.teamcenter.install.tem.struct.TcFeature.upgrade(TcFeature.java:1087)
com.teamcenter.install.tem.director.actions.UpgradeAction.execute(UpgradeAction.java:25)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:143)
com.teamcenter.install.tem.director.Director.run(Director.java:134)
java.lang.Thread.run(Thread.java:744)

The file business_model_updater_2016_11_21_19-05-17.log from the same archive contains the error
Element Name: Fnd0WSOThread
Error: 226534 The value of the attribute "parentClassName" can not be changed

 

Please, review the attached logs, please help me understand why these errors occur and if possible, please provide hints about how to solve these errors.

   
I also tried to install TeamCenter server 11.2.0 from scratch (populating Teamcenter data from the existing Oracle database),
but in this case I obtained the error below (contained in the attached file install_config1_1611211922.txt)


Executing ["/opt/tc/Siemens/Teamcenter11_10/bin/manage_model_files" -u=infodba -p=***** -g=dba -force=model -option=download]
Output from command:  "/opt/tc/Siemens/Teamcenter11_10/bin/manage_model_files" -u=infodba -p=***** -g=dba -force=model -option=download
Fatal Error: Top level std::exception handler called. Caught  exception: Use askUserMessage ( ) or askSyslogMessage ( )
command_exit=1
Exit Status  1, elapsed time 0:00:05
An error occurred during execution.  Stack trace follows...
com.teamcenter.install.tceng.base.DatabaseSteps.manageModelFiles(DatabaseSteps.java:3234)
com.teamcenter.install.tceng.base.DatabaseSteps.manageModelFiles(DatabaseSteps.java:3265)
com.teamcenter.install.tceng.base.DatabaseSteps.install(DatabaseSteps.java:312)
com.teamcenter.install.tceng.base.Foundation.install(Foundation.java:194)
com.teamcenter.install.tem.tasks.JavaTask.execute(JavaTask.java:162)
com.teamcenter.install.tem.tasks.Task.execute(Task.java:128)
com.teamcenter.install.tem.tasks.blocks.CodeBlock.execute(CodeBlock.java:201)
com.teamcenter.install.tem.struct.TcFeature.processAction(TcFeature.java:1407)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1345)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1245)
com.teamcenter.install.tem.struct.TcFeature.process(TcFeature.java:1159)
com.teamcenter.install.tem.struct.TcFeature.install(TcFeature.java:1079)
com.teamcenter.install.tem.director.actions.InstallAction.execute(InstallAction.java:29)
com.teamcenter.install.tem.director.DirectorScript.execute(DirectorScript.java:143)
com.teamcenter.install.tem.director.Director.run(Director.java:134)
java.lang.Thread.run(Thread.java:744)

 

Best regards,
Corina

1 REPLY
Highlighted

Re: Issues when upgrading from TC server 10 to TC server 11.2.0

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

The business_model_updater_2016_11_21_19-05-17.log shows these errors:

 

====================================================================================================================================
Unprocessed Schema Changes:
====================================================================================================================================
Action | Element Type   | Element Name                   | Error # | Error                                           | Template Name
-------|----------------|--------------------------------|---------|-------------------------------------------------|--------------
Change | TcClass        | Fnd0WSOThread                  |  226534 | The value of the attribute "parentClassName" can| foundation   
       |                |                                |         | not be changed.                                 |              
Change | TcClass        | Schedule                       |  226534 | The value of the attribute "parentClassName" can| foundation   
       |                |                                |         | not be changed.                                 |              
Change | TcClass        | ScheduleRevision               |  226534 | The value of the attribute "parentClassName" can| foundation   
       |                |                                |         | not be changed.                                 |              
Change | TcClass        | ScheduleTask                   |  226534 | The value of the attribute "parentClassName" can| foundation   
       |                |                                |         | not be changed.                                 |              
Change | TcClass        | ScheduleTaskRevision           |  226534 | The value of the attribute "parentClassName" can| foundation   
       |                |                                |         | not be changed.                                 |              
Change | TcClass        | WorkspaceObjectThread          |  226534 | The value of the attribute "parentClassName" can| foundation   
       |                |                                |         | not be changed.                                 |             

 

I would send this information to GTAC for them to look into. PR #7617605 and SFB-Teamcenter-9888 allude to certain unsupported upgrade paths, so you may want to check to see if you have to perform an intermediate upgrade to a higher version of 10.1.x before upgrading to 11.2.0.

 

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC