Cancel
Showing results for 
Search instead for 
Did you mean: 

It is possible to view Outlook *.msg dataset?

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

When i attach MS Outlook *.msg file as a Outlook Dataset, there are possibility to view this message into TC or should I use export and open outside Teamcenter?

 

Best regards

Bernard Pacula,
CAMdivision Sp. z o.o.
Consultant PLM/System Architect
2 REPLIES

Re: It is possible to view Outlook *.msg dataset?

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

You can set the viewer of that dataset to be the same as for the html dataset.

this will open the msg file in outlook

but it will open it in outlook outside of Teamcenter viewer

Re: It is possible to view Outlook *.msg dataset?

Siemens Phenom Siemens Phenom
Siemens Phenom

On Windows the msg mime type is usually connected to Outlook and you should be able to view your mail by double-clicking the Outlook dataset. As msg has binary format I don't see an easy way to display it e.g. in the viewer.