Cancel
Showing results for 
Search instead for 
Did you mean: 

Item Creation from AWC 3.0

Experimenter
Experimenter

Hello everyone

 

I work on AWC 3.0 for client with special needs because he don't use items revisions on some of his custom items. He only display the master item for these one. 

So when creating these items with AWC he would see only masters. Currently when I create an item with AWC, it displays the first revisions and not the master item as expected. 

durawc.png

The default behavior, in RAC, is to display only (master) item when user creates a new item. And it is configured with Preferences. 

 

So why this behavior is not reproduced into AWC? And it is possible to display master item instead of revision during AWC item creation?

 

Regards

1 REPLY 1

Re: Item Creation from AWC 3.0

Valued Contributor
Valued Contributor

Hi,

 

AWC add option creates both item and Itemrevision, but the structure is not same as in Richclient. 

 

May be we wait for code changes and they will implement this use case.

 

Regards,

Chene