Cancel
Showing results for 
Search instead for 
Did you mean: 

JT Translator for Solidworks 2018 not showing patterned and/or mirrored parts/assemblies

Experimenter
Experimenter

When I export a JT, using the JT translator for solidworks 2018 we get all the parts into one model. But the duplicated parts by using functions like mirror and pattern are not shown!

JT not showing patterns on different levels

Were do I find an overview explaining the different options you can set in the JT translator config, hereby our current config:

2019-06-20 - JT not showing patterns 01.jpg

version "EAITranslator" 1.0.0 "EAITranslator"

EAITranslator {

               OutputDirectory = "./"

               chordalOption = "RELATIVE"

               structureOption = "MONOLITHIC"

               writeWhichFiles = "ALL"

               pmiOption = "NONE"

               JtFileFormat = "10"

               triStripOpt = false

               seamSewing = false

               seamSewingTol = 0.001

               includeBrep = true

               autoNameSanitize = true

               updateChangedPartsOnly = false

               writeAsciiAssembly = false

               singlePartsNoAssem = false

               autoLowLODgeneration = true

               smartLODgeneration = false

               numLODs = 3

               verboseReporting = false

}

Filter {

}

Metadata {

}

               LOD "1" {

               Level = 1

               Chordal = 0.001

               Angular = 20.0

               Length = 0.0

               AdvCompressionLevel = 0.0

}

               LOD "2" {

               Level = 2

               Chordal = 0.002

               Angular = 0.0

               Length = 0.0

               FeatureSuppression = 0.0

               Simplify = 0.4

               AdvCompressionLevel = 0.5

}

LOD "3" {

               Level = 3

               Chordal = 0.009

               Angular = 0.0

               Length = 0.0

               FeatureSuppression = 0.0

               Simplify = 0.1

               AdvCompressionLevel = 1.0

}

SolidWorks {

               AssmLevelFeatureInstancing = false  --> pattern test true op 20/06/2019 geen verbetering in de patterns

               PartAssemblySelection = "VisibleOnly"

               Configuration = ""

               CoordinateSystem = ""

               GetCustomInfoProps = 0

               appendCADExtension = "NONE"

               LogReporting = "NONE"

               ConsoleReporting = "NONE"

               LogFileName = "SW_PART"

               GetConfigSpecificProps = 0

               GetCADProperties = "ALL"

               XTbrep = true

}

 

1 REPLY 1

Re: JT Translator for Solidworks 2018 not showing patterned and/or mirrored parts/assemblies

Siemens Genius Siemens Genius
Siemens Genius

Hi,

 

In a help section..?

At least JT Bi-Directional Translator for CATIA V5 13.2 have this within installation:

C:\ugs\JTTranslators\CATIAV5\13.2\help\jt_catiav5_help.pdf

 

 

Best regards,
Miloslav Weitz, Siemens PLM Software
Production: Teamcenter 11.5, NX 12, Geolus 9.1
Development: N/A Testing: Teamcenter 12.2, NX 1876, Geolus 10.0