Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

JT checking in the workflow

Pioneer
Pioneer

Hallo Everyone,

 

i want to check with WF, if ItemRevision cointans JT file.

If yes, than give it a status (e.g. Status E) 

If not, than display error mesage (e.g. Itemrevision 008923/A.001-Part4 doesn´t have JT).

 

All this I want to check by multiselect (i.e. before checking and status giving I select ItemRevisions: Product1, Part1, Part2).

 

Any Idea?

Thx.

 

 

 

 

2 REPLIES 2

Betreff: JT checking in the workflow

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

To check JT under IR use the following handler in a validation task:

EPM-check-related-objects
 
-include_typeItemRevision
 
-secondary_typeDirectModel
 
-relationIMAN_specification

In case of failure route to a do-task to display a message as you want.

 

If the JT-dataset part of the workflow target objects, it gets the status.

 

if you sent more than one IR in the workflow, you have to send every single IR to a sub workflow and do the check there.

Michael
Teamcenter UA | NX CAD

Betreff: JT checking in the workflow

Siemens Phenom Siemens Phenom
Siemens Phenom

In addition to checking for the JT dataset, I had to also add a second check for our users to ensure that an actual JT file was attached as a Named Reference.  Maybe somehting to also add for you too.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,