Cancel
Showing results for 
Search instead for 
Did you mean: 

JT to Stp through dispatcher

Legend
Legend

Hi

 

I'm trying to find a way to get a stepfile attached to an item revision in Teamcenter.

As we have Visualization with step translator license I came to think about using it with our dispatcher setup,

OOTB there are no translator to convert JT to step. I have seen that there is a previewservice translator that converts 2D files.

 

Found a document on GTAC describing how to adjust DXF to PDF and was thinking I could use the same for JT to STP.

Has anyone made a custom translator using Visualization or do you think it will be possible to use previewservice to convert a JT to STP if I just add these extension to input and output?

 

Benefit with using dispatcher as I see it is that I get the file export and import plus I can add it to a workflow.

 

Have also tried run EPM-run-external-command in a workflow to get conversion made through Catia but I have some problems to get the script to run. Still investigating this options.

 

5 REPLIES

Re: JT to Stp through dispatcher

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Did you consider using a workflow?

 

Check out page 382

 

Re: JT to Stp through dispatcher

Legend
Legend

Hi

 

Thanks for the reply and yes, this is what I have thought to use when I know what service on the TSTK I could use.

Still not sure if I can configure one out of the box or if I need to create a custom translation service and this I have no knowledege about.

Searched for custom translation as I do thik I have read about it somewhere but not found something yet.

 

At the moment I'm writing some C# code that will manage the translation after I have got the dataset exported to a folder just to get the functionallity to the users. 

Re: JT to Stp through dispatcher

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi

 

You can use JT_Bi-Directional_Translator_for_STEP with the dispatcher.

You do not need to program something, just configure file based translator.

Re: JT to Stp through dispatcher

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Is there a license needed for this?

Re: JT to Stp through dispatcher

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Yes, you need the JT Bi-Directional Translator for STEP [VS22171].