Cancel
Showing results for 
Search instead for 
Did you mean: 

JT translator fails for CATIA v5 R24 data

Creator
Creator

Hello Experts,

 

We have TC 9126, TCIC 903 (with patch to support R24) and CATIA R24.

When We submit CATIA V5 R24 data for catiav5tojt translator, its terminates and does not create JT

 

Any suggestions are welcome

FYR, Below is the module log

 

Translator log messages are in: /TC_DISPATCHERROOT/Stage/DC/Ua7a1217fb5447ec0e490x/result/SIEMENS_catiav5tojt.log
2014-10-22 13:43:02,678 INFO - Standard Input : INFO :
2014-10-22 13:43:02,680 INFO - Standard Error : /TC_DISPATCHERROOT/Module/Translators/catiatojt/v5/UGS/catiav5tojt.sh: line 46: 6768: Abort
2014-10-22 13:43:02,681 INFO - Standard Input : INFO : Siemens PLM JT Bi-directional Translator for CATIA V5, Version 8.2.0 (Build#717)
2014-10-22 13:43:02,682 INFO - Standard Input : INFO :
2014-10-22 13:43:02,683 INFO - Standard Input : INFO : Could not load configuration file : Siemens/JTTranslators/CATIAV5/8_2/EAI_Catia/etc/tessCatia.config
2014-10-22 13:43:02,683 INFO - Standard Input : INFO : Using factory default configuration file : Siemens/JTTranslators/CATIAV5/8_2/EAI_Catia/etc/catiatojt.config
2014-10-22 13:43:02,683 INFO - Standard Input : Caught signal = 11
2014-10-22 13:43:03,681 ERROR - The translation failed because
2014-10-22 13:43:03,681 ERROR - Exit Value = 6
2014-10-22 13:43:03,681 INFO - Translator streams have no errors.

1 REPLY

Re: JT translator fails for CATIA v5 R24 data

Creator
Creator

Solved.

 

For R24 adta , you need to have Catia v5 translator with version 921