Cancel
Showing results for 
Search instead for 
Did you mean: 

Java 9 compatibility with TC

Experimenter
Experimenter

Hello. As the TC/NX admin here I was a bit shocked to hear the company/IS department decided to start using Java 9 starting from the beginning of the next year. We use TC11.2.3 and NX10 at the moment. We have decided to upgrade to TC11.4 and NX12 but alas, budget dictates this will happen maybe in Q2/2019. My question, then, is where to find info on Java compatibility with our current TC/NX version? Is Java 9 supported or do we need to push the Upgrade before the end of the year? Does TC11.4/NX12 support Java 9?

2 REPLIES 2

Re: Java 9 compatibility with TC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The release notes of each product contain the system requirements, here are the ones for NX 12.

You can also search the solution center for the SFBs ( Software Field Bulletins ) about Java and Teamcenter or Java and NX.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Java 9 compatibility with TC

Experimenter
Experimenter

I tried finding info from the solution center but somehow missed these. Thank you! Although...it seems our situation is a bit sketchy if Java 9 is only supported in TC12. Thanks again for the quick reply!