Cancel
Showing results for 
Search instead for 
Did you mean: 

License error on dispatcher request for JT translation

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

I've installed TC 11.2.3 Rapid Start on a customer. Also dispatcher server and client.

Installed 4 tier rich client on a client computer.

I tried to convert a ugmaster to jt with dispatcher client, it sends the request, I see the request on the server, when it tries to start conversion, I get an error in the log file.

 

+++ ERROR : License unavailable.

 

 

This is their license on the server

111.png

 

What can be the problem?

 

Cem

2 REPLIES

Re: License error on dispatcher request for JT translation

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
There are 2 TCADMIN licenses. One is for "infodba" and the other is for "dcproxy". If you use a different name than "dcproxy" then it will require its own TC10101 license. If you stick with "dcproxy" then it will use the TCADMIN license and not require a TC10101.
Note: In order to run the converter, Dispatcher needs to start NX and will pull an NX license. Beyond the TCADMIN license for Teamcenter, you need an NX license that can run/author the translator.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: License error on dispatcher request for JT translation

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

What is the minimum requirement for an NX license for this translation??