Cancel
Showing results for 
Search instead for 
Did you mean: 

MCO workflow issue

Valued Contributor
Valued Contributor

Hi, I got one issue where the warning message occure when I release the MCO object, not error message.

It seems that if the two sessions were runnning on the one client machine, this message was occured.  

 

But this issue is not occured when I run one session  on one clinet machine.

Do you have any idea about this error?

- What is the root cause of this issue?

- How to solve this issue?

 

 

I am not sure why this happen....

 

 

3 REPLIES

Re: MCO workflow issue

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Can you include the warning message text or a screenshot? You haven't given us much to work with.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: MCO workflow issue

Valued Contributor
Valued Contributor

I am sorry. 

 

The warning message is "The initial action was successful. For additional details,  addtiona errors are includedd in error stuck."

 

This warning messeag is occured when I click on the "Aproved" on  Task " Final Approver". 

After that, the object can have release flag.  

 

I guess rest of the task which are background process has fild?

The log is not useful in this case. I don't know what is the root cause of it.

 

 

 

Re: MCO workflow issue

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor
Any automated steps after this "approval" inherit the permissions from the Approver. You can click on "More" when the error message window is encountered to view the error stack. Your investigation should take you through all the handlers from the Complete action of the approval task until the end of the workflow keeping in mind the user's permissions as you go. That's about as much help as I can give you without diving into your workflow.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4