Cancel
Showing results for 
Search instead for 
Did you mean: 

Making an attribute available in Revise dialog.

Experimenter
Experimenter

We added a new property to an Item Revision and made the attribute mandatory to create.

I also wanted to make this attribute mandatory to revise and do not want to carry over value from previous revision.

The issue is that I cannot see the property in the Revise Dialog form. I want the system to prompt for the input of attribute while revising as during creation.

 

How to make this possible?

Following Property Constants were set for the new property in BMIDE.

  • CopyFromOriginal = False (Because we don't want to carry forward the value from previous revision)
  • Visible = True (To make it visible during creation)
  • Required = True (To make it mandatory to create)

Apart from the above Property Constant settings, we set following values in Operation Descriptor

  • Operation Descriptor - CreateInput
    • Required = True
    • Visible = True
  • Operation Descriptor - SaveAs
    • Required = True
    • Visible = True
    • CopyFromOriginal = False

 We are using Teamcenter 10.1.0.

10 REPLIES

Re: Making an attribute available in Revise dialog.

Gears Phenom Gears Phenom
Gears Phenom

You need to look at setting these on the Revise Operation Descriptor. 

 

Jamie

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Making an attribute available in Revise dialog.

Experimenter
Experimenter

I could only see CreateInput and SaveAsInput descriptors in BMIDE.

I'm using BMIDE v10.1.0

BMIDE Operation Descriptor.png

 

What am I doing wrong :( ?

Re: Making an attribute available in Revise dialog.

Gears Phenom Gears Phenom
Gears Phenom

You aren't doing anything wrong. I forgot this wasn't added until 10.1.4 or so. I don't have a template that old to help but look at the BMIDE documentation for Deep Copy Rules and revision. Also look at your revise stylesheet.

 

 

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Making an attribute available in Revise dialog.

Experimenter
Experimenter

Thanks Jamie.

Our Teamcenter version is 10.1.6

Will BMIDE v10.1.4 compatible to Tc 10.1.6?

Can I use BMIDE v10.1.4

Re: Making an attribute available in Revise dialog.

Gears Phenom Gears Phenom
Gears Phenom
I just did a search, it came in 10.1.5. Has your BMIDE template been updated to your current 10.1.6? I’d say you need to update BMIDE to the same version of TC you are using.
Jamie Griffis | Teamcenter Architect | Applied CAx, LLC

Re: Making an attribute available in Revise dialog.

Experimenter
Experimenter

Hi Karthikeyan,

 

Did you got the solution for bringing the attribute in revise dialog ?

 

If yes how did you got that ?

I am also facing same issue.

 

I am using TC11.3

Re: Making an attribute available in Revise dialog.

Experimenter
Experimenter

Yes. This is resolved for me.

As you are using TC 11.4, you can find Operation Descriptor for Revise in the Operation Descriptor tab.

You can define your rule there.

Re: Making an attribute available in Revise dialog.

Experimenter
Experimenter

Hi Karthikeyan,

 

Thank you for immediate reply,

But the custom attributes are not coming in the revise dialog even after making visible=true in Operation Descriptor-->ReviseInput-->Property Constants.

 

Regards

Sreevathsa

Re: Making an attribute available in Revise dialog.

Gears Phenom Gears Phenom
Gears Phenom

Did you add them to the revise stylesheet for the item type as well?

Jamie

Jamie Griffis | Teamcenter Architect | Applied CAx, LLC