Cancel
Showing results for 
Search instead for 
Did you mean: 

Managing Form Properties

Genius
Genius

Hello,

 

I would like some pointers on how to accomplish this using the OOTB configuration.

 

1) Control a field (Date,String,UntypedReference) property values to be entered / modified by a specific user or group.

 

Cheers !

 

Teamcenter 10.1.3
TC Visualization 10.1.3 (Custom Patch)
NX:8.5 | NX 9.02 | Catia V5 R2012 | AutoCAD 2015 | In-Context Editor |
9 REPLIES

Re: Managing Form Properties

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
I had exactly this problem to resolve...
Group A can modify the atributes: Material / Erp Number
Group B can modify the atributes: Description / Free text 1
Have you resolved?

Re: Managing Form Properties

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

As far as I know there is no such ability in Teamcenter. The lowest division level for access control is business object. If you want to restrict access to some attributes you have to place it on a form and then restrict access to the form.

Re: Managing Form Properties

Phenom
Phenom

I am not an expert in Access Manager area, but I was wondering if conditions "HasAttribute" or "Has Form Attribute"  could be applicable in this use case ?

Re: Managing Form Properties

Phenom
Phenom

I found use of "Has Attribute" in an OOTB ACL. See the attached screenshot

Re: Managing Form Properties

Phenom
Phenom

@_bzuk_ :  I think you are right. Though conditions are about attributes, the access rule is still being set on business obect.  So I take my comments back Smiley Happy

Re: Managing Form Properties

Genius
Genius

Hello, Thanks for the response,

 

Looks like this is a current limitation with TC and my query was converted to ER.  Still finding out  ways to accomplish this through a workaround. Let you know if i can solve it.

 

Cheers !

Teamcenter 10.1.3
TC Visualization 10.1.3 (Custom Patch)
NX:8.5 | NX 9.02 | Catia V5 R2012 | AutoCAD 2015 | In-Context Editor |

Re: Managing Form Properties

Genius
Genius

Thanks for your input.

 

Got confirmation with GTAC that this is a limitation. We plan to use form object to store these properties. So

for group A the access will be RW on all the properties. for group B RW on few properties is not possible.

 

Cheers!

Teamcenter 10.1.3
TC Visualization 10.1.3 (Custom Patch)
NX:8.5 | NX 9.02 | Catia V5 R2012 | AutoCAD 2015 | In-Context Editor |

Re: Managing Form Properties

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

It's possible to got the current group in a Runtime property? Cause if is possible we can create a stylesheet with visible options

Re: Managing Form Properties

Genius
Genius

Thanks for your response.

 

I know about the hiding the property by stylesheet options. I would like a property to be visible for all the groups but allow only certain groups to Modify the values. Hence this option wouldn't work for us.

 

Cheers !

Teamcenter 10.1.3
TC Visualization 10.1.3 (Custom Patch)
NX:8.5 | NX 9.02 | Catia V5 R2012 | AutoCAD 2015 | In-Context Editor |