Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Manipulate GRM Rules for structure objects in Collaboration Context Tree

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello together,

At the moment I’m  facing the following Issue:

 

It is possible to copy&paste all kind of Object (resources, processes,..) under a structure object in the collaboration context tree.

See in picture A number 1:

 

pictureA.pngpicture A

 To avoid this, I wanted to create a GRM Rule, which restrict the objects under the structure contexts.

Therefore I need the relation between primary object (structure context) and the secondary object (BOMView Revision).

If I look in the detail tab I see the relation “contents” (See in picture A number 1:).

Unfortunately, this relation is not a relation defined in the BMIDE.

If I look on the properties on the structure context (e.g. MEProcessContext) the property contents is a runtime property.(See in picture B)

pictureB.jpgpicture B

 

 

Can anyone help me with that?

 

Thank you and kind regards,

 

Eva

 

 

1 REPLY 1

Re: Manipulate GRM Rules for structure objects in Collaboration Context Tree

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Eva,

    Teamcenter is showing the "contents" attribute, but I think that the actual relation being used is IMAN_StructureContent.

    You could try writing your rules for this relation.