Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Manually define Revision Number in Teamcenter

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi Experts

 

May I know which setting I need to modify as infodab so I can let user to manually key the revision number when they revise?

In the mean time I also can click 'Assign' to auto update the revision number.

 

Which mean I will have both option manually type and click assign.

 

 

3 REPLIES 3

Re: Manually define Revision Number in Teamcenter

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi @Arisy ,

 

In the default system yes it is possible , there is no mandatory situation to click assaign button. Please check the below pics.

 

2019-03-22_13h21_21.png  For that example , when i'm creating a item , i type manually the revision number such as "00" . Then if you want to revise it , it will go on with the rev number "01".

2019-03-22_13h22_43.pngFor that example , when i'm creating a item , i click the assaign button to give the rev. automatically.

 

If i understand you wrong , please inform me to check the details.

 

Best Regards

Gurkan

Re: Manually define Revision Number in Teamcenter

Siemens Phenom Siemens Phenom
Siemens Phenom

You may be thinking of the ASSIGNED_ITEM_REV_MODIFIABLE preference;

 

000257.jpg

 

This is from the 12.1 Administration Data Report located here.

Browse to preferences / preferences and you'll find it in the list.

 

Re: Manually define Revision Number in Teamcenter

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Hi Experts

Can i restrict this behavior of modifying Rev ID to a particular type rather than making it applicable to all types.

Best regards

Lobo