Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Multiple items (Solid Edge assembly) files in a single ItemRev

Experimenter
Experimenter

In Teamcenter RS 10.1.6 users are able to have multiple files of the same type in a single itemRev.

Example 2 assembly files. Can I prevent this using GRM rules or is there a better way to do it?

 

 

4 REPLIES 4

Re: Multiple items (Solid Edge assembly) files in a single ItemRev

Genius
Genius

Check Multifield Key functionality, this allow you to have two or more the same iteam ids with different multifields.

SE ST9 + TC 10.1.7

UC Re: Multiple items (Solid Edge assembly) files in a single ItemRev

Experimenter
Experimenter

Sorry,
I think you may have got confused. I have a itemtype under Design for SolidEdge data. Within that item type is a part or assembly a draft and pdf plus a file etc..

For some reason it is allowing more than one draft file or more than one assembly file and more than one pdf.

I am trying to stop this from happening so only one draft file or assembly, pdf can be in an itemRev.

I think that I can do it with GRM rules. But I also know that I have to be careful as revising and SaveAs can be effected if not careful.

Tom Deverill BSc (Hons) MBCS - CAD Manager, Design Tech Pubs & MTL

Re: UC Re: Multiple items (Solid Edge assembly) files in a single ItemRev

Legend
Legend

@Rill189

 

Is it possible to place a screenshot to show what you’re encountering...
Possibly also give the information about the data sets within the Item Rev.

Having multiple , PDF or other files types is not uncommon in TC.
However, you should (normally) only have a single 3D Solid Edge data set in each Item Rev.

 

--------------------------------------------------
Marc Boom
marc.boom@outlook.com

Re: UC Re: Multiple items (Solid Edge assembly) files in a single ItemRev

Experimenter
Experimenter

In this example, there are multiple PDF's I need to restrict this to only one.

 

2018-04-13 07_57_50-Clipboard.png

I thought I might be able to restrict using GRM rules?