Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: Multiple languages support in Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

No, I did not ask this question in GTAC.
But I think you should ask it in GTAC if you are going to use Teamcenter 11.x and UTF-8 encoding.

Betreff: Multiple languages support in Teamcenter

Genius
Genius

@ArthurRM

In the best practice from PLMWorld for teamcenter deployment in UTF-8 it is stated that from TC11.2 windows is a supported platform for UTF-8 deployment. I came to the conclusion that the warning is left over in 11.2 installation mistakenly from the 10 version.

see the attach.

BR.

Betreff: Multiple languages support in Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, it is quite possible that this is so

 

It seems that in BCT think the same way:

 

UTF-8 Support for Windows and SQL Server
https://www.bct-technology.com/en/support/tips-tricks/teamcenter-112-whats-new.html

 

But if I continued to work with the UTF-8 encoding, then I would clarify this issue in GTAC. But we refused to use the UTF-8 encoding. Therefore, the need for this has disappeared.