Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Attribute mapping localization

Legend
Legend

Is it possible to use localized attribute mappings in NX? Or attribute name would have only one kind of localization in wich it was enter in?

2 REPLIES

Re: NX Attribute mapping localization

Phenom
Phenom

Good afternoon, I hope I understand you correctly. Yes, you can use the attribute name in NX in your language and use it in the mapping. From the Teamcenter side, you will need to specify the real name of the attribute, as in BMIDE:

 

"Local lang attr name" : ItemRevision.item_id /master=iman /description="Local lang attr desc"

Re: NX Attribute mapping localization

Siemens Genius Siemens Genius
Siemens Genius

if you mean about attributes in nx file then answer is yes, you can.

please, look at ArthurRM answer, keep in mind, that you should only "internal" name for Teamcenter attributes.

All the best, Alexey.