Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Attributes Mapping

Creator
Creator

Dear All,

 

I have two queries on attribute mapping -

 

1. When attributes are mapped from Teamcenter to NX using a mapping file, attributes in New (Create) dialog in NX are NOT displayed in the same order as specified in the mapping file.

Is there any to way set the displayed order of attributes in NX create dialog ?

 

2. When attributes are not marked as required in mapping file, they are not displayed on the main create dialog but are listed in Secondary attributes section. Is there any way to list non required attributes in main dialog ?

 

Appreciate your help.

 

Thank you.

 

Regards

Priti