Cancel
Showing results for 
Search instead for 
Did you mean: 

NX attribute mapping example with /freezable as qualifier

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi There,

 

Anyone knows usage of freezable qualifier in attribute mapping with NX? 

 

According to NX documentation: 

/freezable

An attribute with this qualifier can have its value set by the NX user only if the Dataset does not have a Release Status on it.

 

According to TC documentation:

/freezable

Directs NX to ignore the Teamcenter attribute value, as stored in the Teamcenter database, but to use the value stored in the part file if the related Teamcenter object is frozen.

 

If explaned with use case, it will be really helpful.

 

Thanks in advance,

Sumeet