Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX drawing to PDF

Legend
Legend

Hi

 

I want to create a PDF file of the NX drawing when we save to Teamcenter.

In my dispatcher setup I checked the translator.xml file but there is no nx to pdf setting avalible.

Searched in the helpfiles for NX11 and there it states that an ugtopdf shall be present but it seems to be for Teamcenter Rapid start.

 

2018-01-25_13-46-18-071.png

 

Can anyone share the info about how we can enable PDF creation in the dispatcher for NX, as I can't find the ugtopdf in the installation media for Rapid Start which I have downloaded.

The information above is not complete for the translator.xml file.

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018
1 REPLY 1

Re: NX drawing to PDF

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

To convert NX drawings to PDF, use the nxtocgmdirect translator and modify the batch file to show this set of arguments:

 

"%UGII_BASE_DIR%\Ugmanager\export_ugdwgimages.exe" -all -text=text –pdf -nocgm %*

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC