Cancel
Showing results for 
Search instead for 
Did you mean: 

NX for Active Workspace feature missing in TEM

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello,

 

I have a Teamcenter Rapid Start 11.2.2 installation and will be adding Active Workspace 3.1 to it. Per the deployment guide, I have patched the corporate server and begun the deployment with the first step being picking the server extensions.

 

I noticed that in the deployment guide there are features present which don't exist in my feature list - why is this?

 

Specifically, the feature "NX for Active Workspace" is missing from the list of features available to me but are seen in the screenshot of features in the deployment guide. I have "NX Foundation" extension installed, so NX for Active Workspace should be selectable as feature, but I can't even see it.

 

Is this a software incompatibility between TC Rapid Start and Active Workspace 3.1 or is something else in the works?

 

For reference here is the list of server extensions I can choose from:

 

2016-06-27 10_27_28-TC11 Testmiljö - VMware Workstation.png

 

Thanks.

1 REPLY

Re: NX for Active Workspace feature missing in TEM

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

The "NX for Active Workspace" option is only available with regular Teamcenter, not Rapid Start.

 

I suggest you submit this to GTAC as an enhancement request.

 

-Pat

 

Patrick (Pat) Kennedy, Sr. PLM Application Engineer, Acuity Solutions