Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 version number?

Legend
Legend

What is the version name of NX10 to use in the NX manager integration?

We have defined V26.5 for NX8.5 when we distribute the Rich client through OTW but I'm unable to find the value for NX10.

Someone who knows and can tell were I can this info for the future upgrades or maintenace packs?

 

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018
5 REPLIES

Re: NX10 version number?

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

NX 10, aka NX100, is V28.0.

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: NX10 version number?

Legend
Legend

Thanks Randy!

Where can I find that in NX so I know were to look in future? If we now will un NX NX10.0.1 will it change to 28.1?

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018

Re: NX10 version number?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The version number will not change.

 

The version number is available in the registry at HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Unigraphics Solutions\Installed Applications, look for the number after the keys starting with Unigraphics.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong ;)
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX10 version number?

Solution Partner Honored Contributor Solution Partner Honored Contributor
Solution Partner Honored Contributor

The version number only changes on the main and in between versions. e.g.

if %NX_NUMBER%==NX4   set NX_VERSION=V22.0
if %NX_NUMBER%==NX5   set NX_VERSION=V23.0
if %NX_NUMBER%==NX6   set NX_VERSION=V24.0
if %NX_NUMBER%==NX7   set NX_VERSION=V25.0
if %NX_NUMBER%==NX75  set NX_VERSION=V25.5
if %NX_NUMBER%==NX8   set NX_VERSION=V26.0
if %NX_NUMBER%==NX85  set NX_VERSION=V26.5
if %NX_NUMBER%==NX90  set NX_VERSION=V27.0
if %NX_NUMBER%==NX100 set NX_VERSION=V28.0

 

Best,

/Randy

 


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: NX10 version number?

Legend
Legend

Found also an alternative to see the version number when I went through the Teamcenter log.

The env_print.exe with the switch '-v' will give the version number of the installed NX.

Location:

[UG_BASE_DIR]\UGII\env_print.exe

 

usage: "env_print -all"  will print all variables found in the .ugii_env file
       "env_print environment_variable" will print a single variable
       "env_print -n" will print the NX version number
       "env_print -p" will print the platform string
       "env_print -v" will print the Unigraphics version string
       "env_print -m" will print the patch text string (if it exists)

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018